As with all types of spanner - adjustable or non-adjustable - there are several commonly observed guidelines and codes of best practice you should take note of, in order to make sure you’re using these tools appropriately and safely. These often include such tips as:
Always use a sensibly fitting tool
Try to choose sizes that reduce the amount of play between the jaws and the fastener as much as possible. This will minimise the risk of slipping on the bolt or nut, and potentially damaging either it, the spanner, or yourself
There should never be more than a millimetre of play as an absolute maximum - if there is, you’re not using the right size wrench
Refer to a proper thread gauge if you’re unsure of which size tool you ought to be using for a particular fastener
Don’t try to apply more torque than you can handle
Avoid using hammers, mallets or other striking tools to apply extra torque to any type of spanner that isn’t explicitly designed and built for that purpose (most adjustable wrenches are not)
If you’re placing so much weight on the tool means it is not unlikely that the tool could slip violently or the fastener could suddenly give way.
As it is possible that you’d likely fall or otherwise injure yourself in either of the above scenarios, then you’re not performing the job safely and you may need to consider a different approach.
Be mindful of any existing damage or wear
All tools should always be checked before use for obvious signs of suboptimal condition before tackling any demanding jobs.
Adjustable wrenches ought to be calibrated for width settings on a regular basis, and certainly before starting a new job (even if the fasteners you’re dealing with are the same size as the last time you used the spanner)
Keep adjustable spanners and wrenches clean
In between uses, store them away securely in an appropriate container or tool box to have the best chance of keeping the tools dry and free from excessive grease, grime or rust
If necessary, give them a quick clean before commencing use - this can usually be done with a cleaning rag and some light oil
Be sure to mop up any excess cleaning fluids or oils, as these can also cause hands or spanner jaws to slip while the tool is subsequently in use
Do not use extension bars or tubes indiscriminately
It’s easy to exceed the rated torque specifications of the tool when using extensions carelessly, which can quickly lead to serious damage or injury
Always be aware of your environment
Think about the area you’re working in, and any potential hazards it may pose to you or to other people in the vicinity while completing the task. This can include:
- Available room for manoeuvre
- Prevailing environmental conditions
- Other users of the space
- Potential causes of slips/trips/falls
- Sources of airborne dust, dirt or contamination
- Any other risk factors to your own health or that of others
Consider external factors
Be aware that factors such as vibration or thermal changes can cause sudden loosening or tightening of fasteners, which can be rapidly compounded by any additional forces you’re applying to them