Copper Tape for Plant Pots
Copper tape for plant pots is primarily used by gardeners to keep slugs away from plants. Slugs are pests which can ruin plants if left unchecked, and many gardeners choose to use copper foil tape to deter slugs and keep plants at their best.
The process is simple – merely sticking a strip of copper tape around the plant pot, just below the rim, to act as a barrier. There is discussion around the effectiveness of this method and whether copper tape does actually deter slugs, but many gardeners prefer to try using copper foil as opposed to less environmentally-friendly alternatives like certain slug and snail repellents.
Copper Tape for Stained Glass
Copper tape can also be used in the craft space for working with stained glass. Hobbyists creating stained glass artwork can use copper foil to wrap the pieces, creating a handy guideline to follow when soldering separate pieces together into the final image. Different thicknesses of copper tape are also available, making it easy to select a tape width that suits the size of your stained glass project.
To use, simply peel the tape and place it on the edge of the first piece of glass. Press it firmly down around the edge of the shape, taking extra care if the glass is sharp or jagged. Ensure that each new section of tape you apply overlaps with the last to avoid any gaps.
Copper Tape for Walls
Although copper tape is not intended specifically for use on walls, some people have adopted it as a means of creating attractive, decorative wall art. Due to its high levels of versatility, copper foil can easily be adapted and shaped to suit a variety of patterns and designs.
Geometric designs are common, but there are certainly no restrictions on your creativity! Alternatives include the use of washi tape or simply using masking tape to enable precise, accurate lines between different colours or shades of paint on a wall.
Copper Tape for Crafts
As previously mentioned, copper tape can be incorporated into a selection of different crafts and DIY projects. This can include stained glass artwork and wall art, as explored above, but it can also include a wide range of innovative craft ideas.
Just a few examples include adding a shiny border to artwork, creating textured pieces of art, or combining with other types of tape to create bespoke, metallic creations.
Copper Tape for Paper Circuits
Paper circuits are low-voltage electrical circuits that can easily be created using a selection of common materials. They are often used in DIY or domestic settings, often to teach children about circuits and electrical conductivity.
Copper tape is used to provide the current from one part of the circuit to another. There are numerous different circuit designs you can use for activities like this, but copper tape makes a great addition and is ideal for conducting low levels of electricity around the circuit.