The specific load bank testing equipment and procedure you need to run will change depending on the set-up and type of measurements you require. However, there are some general guidelines you can follow for each type of power source you’re testing, such as a generator, battery, or UPS.
What is a Load Bank for Generator Testing?
Each generator will have manufacturer’s instructions, however, most load bank tests can be conducted using the following steps:
- Connecting the load bank to the generator with the right-sized cables
- Setting the generator’s output breaker to ‘off’ and ensuring the load bank’s emergency stop button isn’t pressed
- Match the load bank’s voltage to the generator’s output, or whatever power output is appropriate for the type of test you’re running
- Turn the control power and load switches on until you reach the right load capacity
- Run the test for your set time before shutting off each of the load switches and, finally, the main power
Battery Bank Load Testing
When you’re load testing a battery, you must follow the manufacturer’s guidelines alongside the following advice:
- Use a DC load bank to run tests on individual batteries
- Make sure you have baseline information (e.g., capacity) that you can measure the test results against
- Be aware of the industry standards that set out battery performance, maintenance, and testing guidelines
UPS Load Bank Testing
Alongside the UPS load bank testing procedure set out in the manufacturer’s guidelines, it’s important to take the following advice into account:
- Use an AC load bank to test the whole UPS
- Run regular visual checks of the individual components, enclosures, and surrounding conditions to ensure any maintenance or efficiency issues are dealt with in advance of problems
- Installing advanced UPS monitoring systems can help technician teams have an overview of its status and alert them of any issues
By selecting the right type of load bank, following the manufacturer’s instructions, and performing these tests regularly, you’ll be able to get an overview of your power source’s efficiency and ensure it will perform well and safely when required.