With a few notable exceptions, peristaltic pumps tend to be on a smaller scale, as they don’t excel in shifting large volumes of fluid quickly. But when controllability, precision and low volume are essential, they are perfect.
One of their most important applications is in the medical setting, where precision and predictable fluid delivery is vital. They are used to pump blood during open heart surgery and for dialysis machines. The pharmaceutical industry uses them in its manufacturing processes for certain drugs, where precise concentrations of certain molecules need to be known so that clinicians can confidently prescribe doses to patients.
The same applies to food manufacturing, particularly to mass production. Once a recipe has been finalised, it needs to be consistently applied in the factory, with precise amounts of ingredients going into the mix. Peristaltic pumps facilitate that precision. If you’ve ever had paint custom-mixed in the hardware store, there’s a good chance the individual dyes will have been injected using peristaltic pumps to ensure the exact shade you’ve ordered.
On a larger scale, some concrete pumps are peristaltic. It’s a useful way of moving wet concrete, full of aggregate, up to heights so it can be poured and produce a single, homogeneous slab, which isn’t always possible with multiple buckets. It also guarantees the heavy concrete mix will not flow back down the pipe when the flow is stopped.