How Do You Cut a Copper Pipe in a Tight Space?
If you need to cut a copper pipe in a tight space, the task must be completed with care to avoid making an uneven cut or damaging surrounding pipework. If possible, it’s advisable to mark out where you want to make the cut before employing the pipe cutting tool as this will help you to make a clean cut, especially if space is tight. You should also make sure that your tool is a good fit for the size of the pipe in order to prevent any slipping or misalignment once you begin to make the cut.
Where space is tight, a single-handed tool is a sensible option as it requires less room to manoeuvre than certain other types of pipe cutter. If you are struggling to access the pipe, a long-handled or ratchet pipe cutter may also make it easier to reach the place where you need to make the cut. When you begin to cut, work slowly with care to avoid causing any potential damage to the pipe’s surroundings. With the appropriate tools, care and attention, you will be able to complete the task.
How Do You Cut Metal Pipe Straight?
It can be tricky to cut pipes straight across, particularly if the pipe is thick or made from a difficult to cut material. One of the simplest ways to cut metal pipe is to wrap a straight piece of tape around the pipe before cutting it. By ensuring the tape overlaps itself, you can simply follow the line created by the edge of the tape as you cut, guaranteeing a straight, even cut. The tape can then simply be removed once the pipe has been cut. This trick is handy if you are looking to cut pipes with a hacksaw, for example.