In the UK, national building regulations say all businesses must have an appropriate fire detection system. This means that in the event of a fire, it should be easy to detect the blaze and warn employees and any other occupants to evacuate. The London Fire Brigade recommends that businesses install a smoke alarm or heat alarm in each room where a fire could potentially start. Fire detection systems should meet the BS 5839 standard which is a code of practice for the design, installation, commissioning, and maintenance of non-domestic fire detection and alarm systems.
BS 5839 recommends the location of components of the fire alarm system. Systems are categorised according to whether they are designed to protect people or property. The standard also specifies which types of detectors should be used. These include not only smoke detectors but also carbon monoxide detectors, heat detectors, and infrared and ultraviolet detectors. Some fire detectors on the market may be multi-sensor, i.e., capable of detecting multiple signs of fire. Smoke alarms or other detection devices should be chosen based on the speed of detection needed, the type of fire hazard, and the need to minimise false alarms.