Sound level meters are instruments for quantifying levels of sound. They are sometimes known as decibel meters (dB meters) or sound pressure level meters. So how do decibel level meters work? They are equipped with a microphone which is calibrated across the audio frequency range. The microphone responds to changes in sound pressure levels which are interpreted onto a digital display via internal electronics. The noise pressure levels are shown in decibels (dB).
You can use them in many environments where noise pollution needs to be monitored or controlled. One example is setting up sound or cinema systems in a public venue. Another is their use in the sound engineering environment. Frequency response and noise levels can be monitored. This will enable you to achieve balanced and quality music recordings.
How accurate are phone decibel meters and do we need a sound level meter? The answer to that depends on what you might want to use it for. Phone apps vary in quality and accuracy. Phones are not all made equal. The bandwidth and frequency response of the microphone being used will vary from one phone to another. When it comes to measuring sound levels with accuracy and consistency then a dedicated sound level meter is the way to go.
Our human ears perceive sound differently from the actual sound pressure levels present and typically they do not follow a flat frequency response curve. We tend to be more sensitive to frequencies of sound ranging from around 500 Hz up to around 8 kHz. For this reason, any meaningful sound pressure readings need to be weighted in favour of that frequency bandwidth. This is so that the sound that we are measuring is pertinent to the frequencies that we perceive the most.
There are three weightings used in sound level monitoring.
- (A) weighted - frequency of 500 Hz up to 8 kHz. This is the humans' most sensitive range and the most used scale. The units of measurement are termed dBA.
- (C) weighted - frequency of 31.5 Hz up to 8 kHz. This scale is used when high-energy bass or low percussive sounds are present; the human ear is more sensitive to lower frequencies at high levels. The units of measurement are termed dBC.
- (Z) weighted - frequency of 8 Hz up to 20 kHz. This is the audible flat frequency response curve. It is useful in the design of audio equipment and where wider, flat bandwidth measurement is necessary. The units of measurement are termed dBZ.