Thumb screws (sometimes written as thumbscrews) are multipurpose fasteners designed to be tightened and loosened by hand, rather than needing tools like screwdrivers or wrenches for installation. They have a wide range of useful applications, especially in parts, materials and builds that do not easily support the use of manual or power tools. This is often due to space restrictions.
Thumb screws and thumb screw bolts can also be useful solutions in a situation where you may need to remove a component or panel regularly. They can make tasks such as maintenance or cleaning much quicker and easier than having to use a driver to remove fully torqued machine screws, bolts, or rivets.
Various sorts of fasteners and fixings might fall under the broad thumb screws definition. A true thumb screw or bolt can be distinguished from standard bolts or rivets by its large head, offering easier grip. They will often have knurled edges around the head section too, further improving friction and purchase while being turned by hand. They may or may not feature a slot in the head for a screwdriver to be used if preferred. Washers are not normally needed with this type of fastener.
Knurled Thumb Screws
Knurled thumb screws are commonly chosen because they give the user a better grip on the head of the fastener when installing by hand.
Knurled bolts and screws of this type are so-called because of the knurling pattern - a series of machined ridges or bumps - found around the screw head. Knurling is a widespread manufacturing technique for improving grip or torque force on a huge array of hand-installed components and fasteners.
Knurled head thumb screws are one of the most common applications of this technique, which can be found on many types of stainless steel or nylon nuts, screws and bolts. The pattern of bumps, ridges or notches allows for much-improved friction between fingers and the otherwise smooth edges of the thumb screw.
Thumb Screw Knobs
Thumb screw knobs, often referred to simply as thumb knobs, are closely related to thumb screws. However, they are specifically designed to be used as quick, easily removable fastener solutions for tightening something down and releasing it on demand.
Examples of typical applications include instrument panels, case lids, battery compartments and enclosure windows. A thumb knob may also be listed as a star knob, depending on the precise shape of the head designed for gripping by hand.
The head section on a thumb screw knob will often be made of plastic (nylon) or resin (Yuliya resin thumb screws are common) and manufactured as a separate piece to the metal threaded section of the screw-in shaft itself. Indeed, nylon knurled head knobs can often be bought on their own, with the heads intended to be press-fit onto thumb screws for easier installation and removal.