Though MIG and TIG welders are widely used for most industrial applications, shielded metal arc and flux-cored arc welding help to meet specific requirements.
Shielded Metal Arc Welding
Also known as stick welding, shielded metal arc welding works by creating an arc between the welder’s consumable electrode and the piece of welding metal. The high temperature created melts the electrode and creates the weld which then joins the pieces of metal together when cooled.
This welding method is lower in cost than other types. The welder is also smaller and more portable, making it more appropriate for welding in restricted spaces and difficult positions, and for moving from one job to another. However, more mess is created and less welding material is deposited per minute, meaning using this process can be less productive.
Flux-Cored Arc Welding
Most used outdoors or on contaminated materials, the arc in this type of welder is created between the metal being welded and the fed consumable filler wire. The core is made of materials that release shielding gases and flux, meaning the weld is protected from any contaminants or flammable gases in the air.
This feature means that flux-cored arc welding is appropriate for use outdoors or wherever wind or drafts may reduce the supply of shielding gas by other methods. Plus, the high deposition rate means this method can quickly produce high-quality welds. There are some downsides, such as the large amount of noxious fumes created, the amount of mess produced and the fact that it's not suited to all metal types.