Because FireWire and USB connectivity is similar to the use of cables and ports, a mistake may be made in thinking that USB and FireWire are different versions of the same technology. However, the truth is that they have largely different abilities, with FireWire having a few advantages of USB connection.
The first advantage that FireWire has over USB is its speed. Both are competitive in the speed of data transfer, but in the case of FireWire 800, the speed of data transfer is much greater when compared to USB. Additionally, FireWire also transfers more data than USB, which makes it a more useful connection on devices such as digital cameras.
Secondly, FireWire has more versatility than USB. Because FireWire comes in power options, they don’t always need a computer connection in order to communicate and transfer data. USB does not have a power option, so relies on the power from a laptop or computer device to transfer data. USB is described as host-based whilst FireWire is peer-to-peer based.
The only disadvantage to FireWire is that due to its usability, it is often more expensive than USB. Even so, if you need a connection for fast and large data transfer, FireWire may be a better choice than USB.