Login / Register to access your benefits
Recently searched
      • Published 17 Jan 2023
      • Last Modified 29 May 2024
    • 21 min

    An Introductory Guide to the IIoT

    Discover more about the Industrial Internet of Things, including its uses and benefits, in our introduction to IIoT.

     IoT Banner

    Reviewed by Jay Proctor, Technical Support Team Leader (June 2021)

    In this introduction to Industrial Internet of Things and Industry 4.0, we will examine the IIoT for industry. We will explain what it is, how it impacts industrial technology, as well as the opportunities and challenges of the recent technology revolution.

    What is the Internet of Things?

    IoT Devices Connected to the Cloud

    The Internet of Things (IoT) is a term used for any device connected to a network (including the Internet) that can communicate autonomously without human intervention. Essentially, it is a connected infrastructure where almost every type of machine and device has built-in intelligence capable of transferring data and interacting with other machines, and via these devices, with people.

    In the consumer space, the term was first used to describe digitally connected products and devices. Nowadays, IoT for industry is often referred to as the Industrial Internet since it has the potential to transform both industry and society, in a similar way to the first industrial revolution.

    What is the IIoT?

    With the IoT definition above in mind, what is the Industrial Internet of Things? IIoT stands for Industrial Internet of Things, describing how the same concept of IoT can be used in manufacturing or other industrial processes. It uses the concept of networking devices and connecting them via the internet to share data locally and remotely in factories, industrial buildings, and industrial processes. This forms the backbone of Internet of Things industrial automation.

    Smart equipment and machinery can track, log, display, monitor, and adjust itself as required. Sensors collect the information, which is consolidated via a gateway through the local network, then onwards through an edge controller to the Cloud or the internet.

    IIoT vs IoT

    The key distinction between IoT and IIoT lies in the application. Industrial IoT centres around the collection and analysis of real-time granular data from connected sensors, enabling rapid improvements in productivity and efficiency, instantaneous stock control, and significant cost savings.

    An established approach to computer-controlled manufacturing underpins industrial IoT: the ‘distributed control system’. The control functions are distributed across the network and multiple autonomous devices are interconnected, making them able to adjust and optimise their own section of the manufacturing line without centralised control and the associated risk of a single-point failure. The IIoT takes advantage of modern cloud computing to allow data sharing, visualisation, and analysis – all near-real time.

    Over the past few decades, the Industrial Internet of Things has grown into a huge sector. Over 60 per cent of global manufacturers now use IIoT technologies for optimisation and analysis.

    This distinction highlights the difference between IIoT and IoT in manufacturing and industrial applications. It is also pertinent to note the comparison of the Internet of Things vs Industry 4.0.

    What is the Difference Between Industry 4.0 and the Internet of Things?

    You may also have heard the term Industry 4.0 in relation to the IoT. Despite sometimes being used interchangeably, the two are not synonymous because Industry 4.0 includes both IoT and IIoT.

    Industry 4.0 is a broad term which encompasses the accelerating use of - and benefits derived from - all the innovations in automation now available to industry and smart manufacturing, such as:

    • Seamless cloud computing
    • M2M (machine-to-machine) communication
    • Autonomous systems implementation
    • Image recognition and other 'cognitive' technologies based on artificial intelligence

    The History of the IoT and Industry 4.0

    The Internet of Things may seem like a very modern concept but some of the core Industry 4.0 technologies date back to the 1960s. The programmable logic controller (PLC) - effectively an early industrial computer - was invented in 1968 and designed to fine-tune the manufacturing process. The first distributed control systems for industrial settings appeared in the 1970s, sparking the gradual supplementation of manual labour with automation within factories.

    The Internet of Things as we know it today first came into focus during the following decade. However, it was not until the early 2000s that the IoT moved out of university laboratories and into purchasable products. This growth was accelerated by the development of enabling technologies like Bluetooth, near-field communication (NFC), and 4G/5G cellular networks.

    Further developments followed in the 2000s, including the creation of now-ubiquitous cloud computing technologies which accelerated the evolution of the IIoT.

    Who Coined the Term IIoT and Industry 4.0?

    We know where the Internet of Things originally came from, but it is tricky to pinpoint who coined IIoT.

    The term ‘Industry 4.0’ was coined as recently as 2011 by the German government to encourage the use of information technology in manufacturing. It was intended to suggest that modern automation and data-sharing technology are equal in significance to three previous industrial revolutions, namely:

    • The development of steam and water-powered manufacturing technology in the latter half of the 18th and first half of the 19th Century
    • Widespread electrification, alongside the spread of railways in the 19th century, enabled multiple technological and industrial developments. The telephone, the automobile, photography, and motion pictures all appeared between 1870 and World War One
    • The digital revolution - i.e. the creation of modern IT in the second half of the 20th Century

    We may not know who coined the term ‘Industrial Internet of Things’ for certain. However, the name ‘Industry 4.0’ makes logical sense and boosts understanding of the meaning behind the concept.

     IoT Structure Diagram

    What is the Industrial Internet of Things Used for Now?

    Industry 4.0 can bring benefits to a broad spectrum of industries and sectors.

    Just a few IIoT applications and examples include:

    • Smart factories
    • Supply chain and inventory optimisation
    • Data analytics
    • Smart buildings
    • Condition monitoring

    To understand how IoT will impact different industries in the future, it is important to understand how the manufacturing industry uses IIoT now. Of course, manufacturing is not the only sector to benefit from Industry 4.0. It’s also clear to see how IoT is transforming the energy industry and the retail industry with connected devices and smart systems.

    The Effects and Benefits of the IIoT in Manufacturing

    So, what benefits does the Industrial Internet of Things have in manufacturing? Let’s look at a few examples of how the manufacturing industry uses IIoT:

    • Optimising the manufacturing line: Industrial IoT sensors enable continuous monitoring of the production line from start to finish. This enables operators to continuously fine-tune the manufacturing process, saving time and money
    • Inventory and supply chain management: manufacturing relies on the availability of raw materials and components. RFID (radio frequency identification) tags and similar technologies allow components and supplies to be tracked continuously, in real-time, from location to location, providing continuous monitoring of inventory and compensatory adjustments
    • Packaging assessment: Industrial IoT sensors allow manufacturers to monitor packaging condition during transit and storage and even assess how customers typically interact with it, enabling improvements to design
    • Real-time manufacturing data: IIoT devices can supply real-time operational data to suppliers, enabling responsive adjustments and remote management of factory units
    • Maintenance data: Industrial Internet of Things devices can issue alerts when faults occur and maintenance is required. Similar alerts can be issued in response to operating issues, such as higher-than-recommended operating temperatures or excessive vibration, which could indicate an impending hardware failure. These alerts provide clear advantages in allowing maintenance to be scheduled in advance, minimising downtime and lessening accident risk. Such data can be combined with health and safety records to improve overall safety
    • Quality control: IIoT data from multiple sources, including suppliers, manufacturing processes and end-users, can all be combined to enable overall improvements to product design and production

    What are the Challenges of Industry 4.0?

    This is a complex question with no easy answer.

    As with any huge technological change, there is a lot of work to be done behind the scenes to make these changes a reality in everyday life. Many companies are working to ensure that the underlying infrastructure and connectivity can support the IoT, for both wired and wireless connections.

    As the world becomes more interconnected, we become more dependent on networks. It is also essential to ensure that suitable regulations are in place and fully observed.

    At its broadest, Industry 4.0 is a configuration of multiple networking technologies, so the biggest challenges focus on the maintenance of strong and secure inter-device connections. This is achieved via:

    • Selection of robust, fit-for-purpose networks – either wireless or wired
    • Adopting protocols which promote inter-operability e.g. OPC UA
    • Maintaining vigilance about network security to ward off cyber threats

    As a result, the principle challenges of the IIoT similarly revolve around data storage and digital security. There are privacy and security concerns at all levels. Technology will allow access to unprecedented amounts of data, and everyone involved will need to be vigilant and resilient to ensure this data remains secure.

    In addition, there are additional technological requirements posed by the constant need for uninterrupted device connectivity. It is also imperative to understand security considerations and challenges in adopting the IIoT to ensure a smooth, efficient implementation.

    So, what are the risks associated with IIoT?

    As with all aspects of the digital environment, cybersecurity is crucial for the Industrial Internet of Things. Many consider the primary risk associated with IIoT to be online security, yet security issues are rare. Taking precautions, practising cyber security, and maintaining a secure system are the keys to avoiding IIoT risks while making the most of connected system benefits.

    With that in mind, it’s critical to keep abreast of the latest technologies and updates to stay prepared and protected as the Industrial Internet of Things continues to evolve.

    IoT Potential: What is the Future of the IIoT?

    Both the Internet of Things and the Industrial Internet of Things are constantly evolving. As the latest technologies become available and businesses become increasingly interested in IIoT benefits, more possibilities open up. This also brings numerous predictions about where the Internet of Things is heading in the future.

    While it’s difficult to know exactly what the future of IIoT holds, digital connectivity has the potential to change industry and impact businesses around the world.

    For instance, in the near future, we may live in a world where buildings automatically adjust their temperature to outside weather conditions. Industrial refrigerators could restock themselves according to ingredient lists specified by chefs, or vehicles in a garage could automatically order parts as required.

    These smart, networked devices will be able to publish data on the Internet. This information could be used in various ways to improve the products and services we use every day. It will provide the basis for smart grids and connected cities, improving energy use and consumption, traffic flow, and services for the public.

    The IoT could solve numerous problems in two major areas - power and healthcare. For example:

    • Buildings waste more energy than they use. With the IoT, this could be reduced to almost zero
    • The IoT could enable continual monitoring of bodily functions without visiting a doctor

    The IIoT is also likely to have a major impact on the logistics industry and supply chains, as objects can transmit their location and therefore be redirected more easily in the event of supply disruption.

    What is IoT Connectivity?

    Companies can take advantage of the new opportunities, business models, and revenue streams that are enabled by connectivity.

    Sensors, on-device software, and adjacent technologies are all part of the IoT-connected world that shares data between systems, devices, and physical objects. It is the connectivity between the "things" of the IoT that enables these exchanges to take place.

    Different types of IoT connections are used, depending on individual device requirements. These vary in two contexts:

    1. IoT-connected devices that rarely need to communicate with small amounts of data
    2. Always connected devices with constant connectivity and high-speed, low-latency communication that require large amounts of data

    The Next Level in Artificial Intelligence

    There is a wide range of IoT connections available, which enable you to connect something ranging in size from a dental implant to large vehicles and machinery.

    Linking these various things to the Internet of Things and incorporating sensors provides enhanced digital intelligence. This enables real-time communication between connected devices and participation in large-scale automated processes.

    As the IoT evolves, connectivity accelerates rapidly. Forecasts for Internet of Things devices show an upward trend in implementation with a huge number of interconnected devices.

    Internet of Things Architecture

    Internet of Things Architecture

    The IoT architecture typically refers to three core elements.

    • Things: Any device that connects to a network (wired or wireless)
    • Network: Cloud-based network or gateway connecting multiple devices
    • Cloud: A remote server located in a data centre that consolidates and stores data securely and safely

    These three elements are explored in further detail in the sections below.

    IIoT Networks, Protocols and Connections

    Like any other information technology, the Industrial IoT uses a variety of protocols (data communication formats) and network types. As a result, it's important to clarify each if you plan to create an IIoT infrastructure for your manufacturing premises.

    IoT-connected devices range from simple sensors and actuators (such as turning on or off a light) to complex, always-on devices.

    Monitoring continuously has demonstrated the benefits of IoT in ensuring uninterrupted logistics, for instance. However, more recent industrial internet applications will depend on low-latency and high-bandwidth connectivity to facilitate applications such as video-enabled security or remote medical procedures. Therefore, the types of connections are becoming increasingly diverse, taking into account IoT devices' differing needs.

    From traditional Wi-Fi or Bluetooth to newer LoRaWAN and Sigfox, many languages or protocols are emerging for the IoT. The use of each depends on the following elements:

    • Frequency: Which frequencies are available in the area?
    • Range: Is it necessary to transmit a few metres or a few kilometres?
    • Power Consumption: Wearables, for example, have a short battery life
    • Data Rate: How much data is sent?

    The list of IIoT-suitable networks expands continuously, but key examples include:

    Hyper-Scalable Internet of Things

    Different types of devices and connections are combined to form the hyper-scalable IoT, enabling new innovations and expanding the scope of what is possible.

    LPWAN (Low-Power Wide-Area Network)

    Low-power wide-area networks (LPWAN) typically use unlicensed spectrum radio technology for low-capacity operations on sites like mines, campuses, and factories. The majority offer a low-energy consumption, cost-effective alternative to mobile phone connectivity and are suitable in IoT applications that need a modest operating range.

    LPWAN connectivity types include:

    Wireless access point

    Wi-Fi

    This wireless networking technology has become very familiar to most of us since it became the standard method for connecting PCs, smartphones, and tablets to the internet. It's commonly used for internet access and local area networking of devices in homes, offices, and businesses. Wi-Fi has a range of 20-150 metres with some versions reaching speeds of over1 Gbps. It is a derivative of the established wired Ethernet network and is based on the IEEE (Institute of Electrical and Electronic Engineers) 802.11 wireless standard.

    Bluetooth Dongle

    Bluetooth

    Bluetooth is a short-range communication standard based on ultra-high frequency (UHF) radio waves in the ISM bands, between 2.402 GHz and 2.48 GHz. Bluetooth wireless technology is widely used in consumer applications for creating personal area networks and sharing data between fixed and mobile devices over short distances.

    BLE Development Board

    Bluetooth Low Energy (BLE)

    Bluetooth Low Energy is used in wireless beacons, security, healthcare, and domestic entertainment. As an independent technology of Bluetooth, BLE provides low consumption of power while preserving conventional Bluetooth range.

    Zigbee 3.0 Module

    Zigbee

    Zigbee is a low-power communication protocol developed to create personal area networks. Typical applications include domestic automation, device data collection, and other low-power, low-bandwidth uses. This technology is limited to transmission distances of 10-100 metres within line of sight to keep consumption down. Zigbee has a defined data speed of 250 Kbps and is suitable for intermittent data transmission.

    Zigbee 3.0 is the latest version and is widely used in industrial and factory settings. The related protocol Dotdot was created by the same team and has become an internationally accepted, universal method of secure connection between different Internet of Things devices.

    LoRaWAN

    LoRaWAN

    LoRaWAN (Long Range Wide Area Network) provides two-way secure connections across very large networks. This networking protocol connects battery-operated wireless devices to regional, national, or global networks. Bi-directional communication, security from end-to-end, mobility, and localisation services are all provided. Transmission speeds of LoRaWAN range from 0.3 kbps to 50 kbps.

    Sigfox

    Sigfox

    Developed in France, Sigfox connects low-power, always-on objects like electricity meters and smartwatches, allowing them to continuously exchange small quantities of data. Sigfox is similar to LoRaWAN in that it is a technology designed for global coverage to provide wireless networks to connect low-power objects. With minimal power consumption, it uses 900MHz bandwidth and supports up to 140 uplink messages per day. These messages can carry 12 octets of payload data at 100 bits per second.

    NB-IoT Development Kit

    Narrowband IoT (NB-IoT)

    With NB-IoT, a wide range of IoT devices and services can be enabled by low-power wide-area (LPWA) technology. This technology significantly improves system capacity, device power consumption, and spectrum efficiency, especially when it comes to deep coverage. As an alternative to mobile phone networks, it offers a simpler, lower bandwidth solution.

    IIoT Data Protocols

    Small bytes of data generated by things represent sensed information such as position, humidity, or temperature. Due to its small size, this is commonly referred to as 'little data'.

    As multiple devices send this little data to the Cloud, it is consolidated and tracked over time, often becoming increasingly large. This is what is sometimes called 'big data', and it is where IoT excels. The use of big data allows you to understand, monitor, and control things more effectively by analysing thousands or even millions of data points.

    Events are connected to results or actions through sensor analytics. For instance, it may be a sign of imminent failure if sensors detect increased vibration on a machine. This allows parts to be ordered and predictive maintenance scheduled.

    Common IIoT data protocols include:

    • MQTT (Message Queue Telemetry Transport) is a lightweight, low power protocol used to transmit simple data sets between sensors and applications. It sits on top of the standard internet networking system TCP/IP (Transmission Control Protocol/ Internet Protocol)
    • AMQP (Advanced Message Queuing Protocol) is an international standard focused on the transmission of messages between devices. It is approved as an international standard
    • OPC UA (OPC Unified Architecture) is an open machine-to-machine communication protocol supporting cross-platform industrial automation data sharing and robust interoperability of systems

    “Things” in the IoT

    Connected Devices

    The Internet of Things includes numerous devices. See below for some common examples of connected devices and what they are typically used for.

    • Access Point: An access point is a wireless networking device that facilitates connecting devices in a local area network
    • Device: A device is a piece of equipment or hardware programmed to perform at least one processing function in a system
    • Beacons: Small transmitters connected to Bluetooth or BLE-enabled devices like tracked packages or smartphones
    • Gateway: A "translating hub” that facilitates communication between devices, allowing them to exchange data and communicate with each other
    • Hub: Hubs are hardware controllers that connect a central station to data transmission devices
    • Sensor: A sensor detects input from its environment and converts it into data that can be analysed by a person or machine

    Key Technologies

    What is required for devices and machines to communicate intelligently with the internet? Below is a list of key technologies.

    • Actuator: A device that moves or controls a mechanism or system; opening a valve, for example
    • Cyber-Physical Systems: Systems that integrate networking, computing, and physical processes through feedback loops in which computations affect physical processes
    • Contactless: A technology that connects a mobile phone, smart card, or other device to an electronic reader wirelessly, without physical contact
    • Digital Twins: Virtual replicas of physical devices, systems, places, people, and processes that can be used for a variety of purposes and integrate historical machine data
    • Geofencing: Using GPS technology or RFID to define a virtual geographical perimeter within which devices may operate
    • Geographic Information System (GIS): Used to acquire, handle, analyse, present, and manage geographical or spatial data
    • Global Positioning System (GPS): A technology that enables localisation services
    • Global Navigation Satellite System (GNSS): A satellite constellation that transmits navigation, timing, and positioning data from space to GNSS receivers
    • Haptics: Conducting human interactions with computer applications based on tactile sensations and control
    • Hardware-Assisted Virtualisation (HAV): Using a computer's physical components to create and manage virtual machines (VMs)
    • Inertial Measurement Unit (IMU): Measures angular motion, specific force, and magnetic field of devices, such as drones
    • Light Detection and Ranging (LIDAR): LIDAR is a type of remote sensing technology that collects measurements from laser pulses and uses them to map objects and create 3D models
    • Mechatronics: Combines mechanical and electrical engineering with computer science, and includes robotics, electronics, information technology, telecommunications, product engineering, control, and systems
    • RADAR: A radio-wave-based detection system that determines object range, angle, and speed
    • Telematics: The use of GPS and onboard diagnostics to track assets and log their movements

    Hardware and Software

    The IoT must work in combination with suitable hardware and software, including:

    • eSIM: An embedded SIM complies with GSMA specifications and allows remote management of multiple mobile network operator subscriptions
    • Integrated Circuit Card Identifier (ICCID): The unique serial number embedded in SIM cards
    • International Mobile Subscriber Identity (IMSI): An individual, usually fifteen-digit number that identifies a device connected to GSM
    • IoT Module: An embedded device connected to a wireless network that sends and receives information
    • IP Address: An Internet Protocol address identifies a computer (or other device) on a network
    • Modem: Hardware that allows computers to send and receive data over cables, satellite connection, or telephone lines
    • Router: A hardware device that receives, analyses, and forwards IP packets
    • Wireless Modem: A modem that connects directly to an internet connection via a wireless network, bypassing the telephone system

    FAQs

    How to Start Your IIoT Journey

    Are you ready to begin your IIoT journey? Explore the related product ranges below and kick-start your industrial technology revolution.

    Related Articles

    Related links