Globally, the power module market is growing fast because of the increasing use of electric vehicles and the integration of renewable energy resources onto the grid. MOSFET and IGBT power modules have become the market-leading type of power conversion in recent years and the development of new, even higher-power current output designs of power modules is a key technology future trend. Applications include renewable energy and power transmission.
There are also new high-temperature silicon carbide power modules coming onto the market. These types of modules overcome some of the problems related to differing coefficients of thermal expansion and resulting in thermal-mechanical stresses.
For electric vehicles, more sophisticated designs of power modules are helping achieve higher power density in applications such as converting battery power into three-phase alternating current (AC) to drive the vehicle’s propulsion system. Gallium nitride transistor-based power modules are expected to help enable the next generation of electric vehicles by reducing the size, weight and cost of drivetrains.
So, power modules are not only staples of an industry, they are also proving crucial in the energy transition. That means their importance as a means of power conversion and energy transition is only set to grow in the coming decades as the Better World products continue to decarbonise the economy.
Do you need a power module for your application? RS can help. Check out our range of IGBT modules.